This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用PGA309校正我的电阻桥传感器,校正完成后的结果不对,设定的电压输出是最小0.5V,最大4.5V,校正完成后,输出最小0.055V,最大4.3V,这个结果感觉不对,正确的结果应该和设定的一样,在校正结果中发现GAIN DAC 和ZERO DAC的数值特别大,分别为3.8和2.1,请问各位是啥原因?
是不是你的 电阻桥传感器 阻抗比较大, DAC 系统引起了影响了?
桥式电阻传感器,阻值1.1K应该不大呀,我设置的目标电压是0.5-4.5,实际校正后的输出电压是0.05-4.3.请问您,是十么原因?