Part Number: USB2ANY
Other Parts Discussed in Thread: ALP
使用USB2ANY连接Analog LauncuPAD,接好I2C和GND以后,连接USB2ANY对应的pin,无法识别到953,测量USB2ANY I2C信号(测量时已经断开外部设备,只测量USB2ANY输出),SDA 一直为3V高电平,SCL一直为低电平,USB2ANY 固件版本为2.7.0.0,请帮忙看下这个是什么问题,谢谢。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
点击下面的scan connected devices试试,看是否能扫描已连接的板子型号?
左下角您这里都显示ALP framework-Hardware connected,就说明已经和EVM板正常连接上了。
这样,您在USB2ANY/Aardvark Setup这里(左边蓝色框),打开之后再重新选择Select daughter board添加进去试试。

非常感谢您的反馈。
那这个帖子我暂时就先关闭了,后续有什么问题,再联系。