This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5142DDV的代换

Other Parts Discussed in Thread: TAS5142, TAS5162

请问TAS5162DDV能直接代换TAS5142DDV吗?电路需要改动吗?

  • 你好!

              TAS5162 和 早期 的 TAS51x2 是pin to pin 兼容的,OEM可以灵活替换 : 100 W / 每通道 (TAS5142), 125 W / 每通道  (TAS5152)  or 200 W / 每通道 (TAS5162) , 不需要另外设计。 保证电路和电源的额定输出功率能够支持TAS5162即可。