This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求宽带放大器的设计方案(放大几Hz-20MHz的300uV的信号到1V左右)

Other Parts Discussed in Thread: TIDA-00066

您好:

能否提供一种设计方案能满足如下要求:(1)信号的带宽为几Hz-20MHz;(2)信号源的阻抗为几千欧;(3)信号源的幅度为300uV左右,要求在整个带宽内实现70dB左右的增益,把信号放大到1V左右。是不是需要采用多级放大器,在这么宽的带宽以及高增益的条件下,如何实现低噪声要求。请提供解决方案,谢谢!

  • 亲;这确实需要多级放大。每级放大倍数控制在10以内;四级放大可以达到亲的要求。

  • 你好,如XP所说的,应该考虑采用多级放大的方式,TI有相关的设计可供参考:

    http://www.ti.com.cn/tool/cn/TIDA-00066?keyMatch=%E5%A4%9A%E7%BA%A7%E6%94%BE%E5%A4%A7&tisearch=Search-CN

  • 您好:

    谢谢您的回复,我看了一下这个多级的放大器参考,在几KHz-20MHz增益是可以做的比较高,但是看测试的幅频特性测试曲线,增益平坦度不是太好,尤其是在低频段,该参考设计能否通过降低放大增益和调整(实现单位直流增益的电容)的容值大小来提高低频段的增益?补充输入条件: 源阻抗和负载阻抗都为50欧,源的大小为300uV左右,放大到1V左右。

  • 亲;可以用电容补偿增益不平坦问题。因高频阻抗匹配需要;输入阻抗过低是限制低频平坦的关键。亲;建议首先尝试高频电容并多颗表帖钽电容方式解决输入频带问题,钽电容总量可以达到10000uF,这样就能保证1Hz以上输入信号的平坦问题。

  • 一个很正常的放大需求,问题如下:

    1》几Hz至20MHz的输入AC耦合,下限频率问题不大

    2》20MHz的根号是4472,按照你300uV(RMS还是Vpp?)时候看到的信号是信噪比20db算(示波器看已经是粗粗的线了),你的噪声不能大于30uV(前面的RMS还是Vpp?)如果是Vpp,那么代表4.54uV的RMS噪声,那么折算除以4472,就近似等于1nV每根号Hz的噪声噪声水平,非常非常非常困难。

    你已经说内阻是几k欧姆,1k欧姆是4nV每根号Hz,算4k就是8nV每根号Hz,你源的噪声就这个水平?你如何要求高低噪声?

    3》放大没什么好说的,第一级低噪声,放大10倍,增益积至少200MHz,最好500MHz,去选型中心去选,输入噪声要低于8nV

    后面每一级都是10倍即可,除非你愿意用电流运放,否则这么大的带宽,不要试图用更大的增益,也许20-25-25是个好方案,后面运放用视频运放,带宽可以更高一点