TI工程师,你好!现需要检测图中所示的一个微小电流(正波峰约为15μA,负波峰约为8μA),图中的电容C是为了隔离高压HV。
由于检测的电流信号特别小,要求放大器噪声低,抗干扰能力强,放大器的放大倍数40 dB、带宽200 MHz 为宜,且输入阻抗严格保证为 50 Ω。
请推荐一款放大器。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
运放的输入阻抗一般都很大,满足“虚断”条件,如果输入阻抗只有几十ohm的话,那么输入电流就会流入运放的输入端。
你可以看下OPA657作为I-V前级放大:
FEATURES
●HIGH GAIN BANDWIDTH PRODUCT: 1.6GHz
●HIGH BANDWIDTH 275MHz (G = +10)
●LOW INPUT OFFSET VOLTAGE: ±0.25mV
●LOW INPUT BIAS CURRENT: 2pA
●LOW INPUT VOLTAGE NOISE: 4.8nV/ Hz
●HIGH OUTPUT CURRENT: 70mA
●FAST OVERDRIVE RECOVERY
APPLICATIONS
●WIDEBAND PHOTODIODE AMPLIFIER
●WAFER SCANNING EQUIPMENT
●ADC INPUT AMPLIFIER
●TEST AND MEASUREMENT FRONT END
●HIGH GAIN PRECISION AMPLIFIER
如果需要差分信号输出的话,得用全差分运放了。gang ji2 说:但是TIA应该只有单输出吧,后级怎么接仪放来减少共模干扰?或者差分信号这么产生?
您好,我也在设计微小信号的放大,输入信号是10uV左右,输入频率范围是20Hz~20kHz,是由精密电阻完成的I-V变换,能否在前一级放大时应用OPA657,第二级放大的时候同样用OPA657行吗?还是选用OPA827做两级放大呢?谢谢