This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA128: REF输入电压1.25V,出现一些器件烧毁现象,想知道其额定输入是多少?

Part Number: INA128


电路如图,主要用于热电偶测量(一共有8路),原来设计REF直接接地没问题,后来考虑负温差且AD没有负压测量,所能直接在REF上往上抬电压1.25V,发现有些器件工作正常(没跑全程),有些直接裂开了(出现负电压输出),相知道REF管脚输入的额定电压是多少?

  • 您好,1.25V是可以的,并且您使用的电压参考源提供低阻抗输出的1.25V, 接法是没问题的。

    有更换一片再试试吗?

    另外,这类仪表运放就是要注意其共模输入电压范围,保证其工作在安全范围内。

    可以借助于Analog Engineer's calculator这个计算工具验证下您的当前应用是否在安全工作范围内,下面这是当4.85V供电时,Vref=1.25V的Vcm和Vout的关系。