Part Number: OPA855
Other Parts Discussed in Thread: OPA858,

我的目标是20 nA的电流在100 MHz带宽上放大到至少10 mV级,探测器的电容为10pf。为了提高带宽,我使用了T型电阻网络和两个运放构成AFE。我想提问
- opa855为双极性输入,opa858为cmos输入,似乎使用opa858会有更好地信号的质量,尤其是在电流仅为nA量级的情况下。但是opa855有着更高的带宽,我该如何取舍这些因素。
- 目前我只在TINA上大概实现了50 MHz的10 mV信号(因为我后级有AGC,因此我不是很在乎3dB带宽),如何下一步改进这个电路使他有更大的带宽呢。