Part Number: OPA356
我使用OPA356制作了一个跟随器,输入信号频率为4MHz,使用±2.5V的LDO进行供电,测试起来发现跟随器的输出波形的负半周与输入波形一致,但是输出波形的正半周的幅幅值比输入波形的小,输入信号没有超过电源轨,这会造成我后续计算电路输出一个错误的值,请问这是什么原因造成的,怎么解决呢?波形见下图,蓝色为输入信号波形,紫色为跟随器输出。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
也就是说运放的反向输入端和同向输入端信号波形不一致?
后续电路接和没接都是这个样子
这也就是说与后端负载没有关系;
输入信号是1Vpp DC=0V 的 40MHZ正弦波?我用TINA仿真,运放的输出和输入是完全一直的,所以我想看下您前端输入电路是怎样的?

另外,您测试了几块电路板?都是这种现象吗?