Part Number: OPA657
Other Parts Discussed in Thread: OPA847

如图,两个芯片均为OPA657, 下方未ITA电路;上方未反向比例运放:Rg=1K,Rf=62k,Cf=0;原本反向比例运放是用的OPA847,由于它产生直流偏移,所以想用657来代替,但是焊接好后,发现芯片冒烟了;不知是什么原因。测试过芯片电源引脚电压正常。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

由于847和656引脚兼容(847的8号脚未dis,6568号脚为NC),所以直接贴出板子上847的原理图
您好,我对比了这两款运放,如果考虑OPA657的输出电流大, 那么OPA847的sourcing current也很高。
我想同样如果OPA847的VDD走线够宽,也就是能允许足够电流通过的话,OPA657 问题也不大。
并且同样OPA847和OPA657虽然都是高电流输出,但都不需要加散热器,二者的热阻是一样的。
那对比PIN6和PIn7走线太近(这里确实走线很近),但是OPA847和OPA657的管脚排列是相同的,如果OPA847没问题,657也可以的。
不知您换一片OPA657 试了没?