This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA202: 反向输入

Part Number: OPA202


 您好 请问一下 电路图如图所示 当我R1 R2均为10k时 并且我让OPA202的IN+为0V的时候 IN-处的电压为0.4V 请问为什么会出现这种情况,当我改变R1 R2电阻不相同时(R1 为10k R2为4.7K,在IN+为0V时 此时IN-为0v. 不太明白为什么R1 R2电阻相等的时候 为什么IN-的时候会有0.4V的电压 ?谢谢

  • 您好,

    这应该是OPA202输出电压摆幅的限制造成的。OPA202的输出电压幅值到不了电源轨,具体见下面截图,也就是说在使用±5V给OPA202供电时,比例放大倍数是-1(R1 R2均为10k),输入5V时期望输出是-5V,但是由于输出摆幅限制输出到不了-5V(负电源轨),这使得运放不再工作在线性区反向输入电压不再为0。

    当R1 为10k R2为4.7K,比例放大倍数不到1/2,因此期望输出到不了-2.5V,此输出电压在运放输出摆幅范围内,因此运放工作正常。