Other Parts Discussed in Thread: OPA657

如图,OPA847的输出直流偏置导致高电平到达输出上限电平3.5V,导致信号出现平顶。问题是:为什么不是上面的信号全部出现削顶,例如对于信号的最小值,都是平齐的;感觉上面的峰值,只要有一点超过3V就会直接拉到3.5V的平顶上面去(跳变),请问这是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,输出电压swing是和负载有关系的,datasheet中给出了当负载为400ohm时,+-5V供电,最大输出电压幅值典型值为+-3.5V。100ohm负载条件下的输出幅值典型值为+-3.4V

另外我们可以看下输入共模电压范围VS 输出swing以及供电电压的关系曲线。

通过您的波形来看,平稳的部分都是没有达到输出饱和,也就是运放工作在线性范围内的,输出尖峰您的意思是只要输出高于3V就会被拉到3.5V,那么此时输出高于3V的时候,输入共模电压范围是多少?是否能保证OPA847是工作在线性范围内的?
采用的反向比例运放,共模电压为V-/2,按照输出交流2V计算(847由于Bia 电流会产生1.5v左右的直流偏置),输入约30mv左右,实际上测试反向比例之前的电压也是很小的。另外,共模电压范围VS 输出swing以及供电电压的关系曲线,它的意思是,共模输入小于3.2V左右时,输出摆幅为3.2V吗
您好,上图中使用的是OPA657,问题描述的是OPA847,应该是OPA847对吗?
另外,您提到847能产生1.5V左右的偏置,能说下原因吗?我没看到电路中加偏置电路,或者说OPA847内部有偏置电路导致输出共模电压为1.5V,并且OPA847的bias current为uA级别。
OPA847的典型值:bia current =19uA, Vbias=19uA*62k=1.17V;实际仿真和测试大概是在1.5V左右。
输入+-30mV的正弦波吗?除了输出饱和之外,波形也失真了吧?
不知您输入30mV的什么信号测试的?我用TINA仿真是正常的。

是OPA657,我直接在OPA657的产品主页提供的OPA657 TINA reference model上修改的电路。
这个是iOPA847的仿真,确实输出有个直流偏置电压。但是从示波器测试的图形来看,是失真的呢,实际测试时输入是正弦波吗?

嗯,那可能还是要看下饱和部分的输入电压是多少?是否满足输入共模电压范围。
共模电压范围VS 输出swing以及供电电压的关系曲线,它的意思是,共模输入小于3.2V左右时,输出摆幅为3.2V吗
可以看到比如+-5V 供电,positive/negative input和positive/negative output的范围,可以看到,输出范围输入范围是差不多。