This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2317-Q1: 输出功率和电流问题

Part Number: OPA2317-Q1


How to get the max output power or current while using +5V power supply?

采用+5V单边供电时,怎么知道最大输出功率或电流?

  • 您好,

    您的意思是datasheet仅给出±2.75V供电电压下的输出电流输出电压曲线图,没有给出单电源5V的是吗?

    单电源5V供电时仅将上面曲线的-2.75V看作0V,+2.75V看作 5.5V即可,即纵坐标的参考点变一变。

    ±2.75V与±2.5V电压下的曲线趋势一致,您可用±2.75V曲线估计单电源5V的值。

    希望以上理解了您的问题,解答了您的疑惑。

  • 多谢解答,能解答下为啥可以这么等效么?

  • 上图中给出了±2.75V和±0.9V供电下的曲线图,可以看出它们的曲线变化趋势是类似的,因此 ±2.5V的曲线也与±2.75V的曲线变化类似。

    您采用单电源5V供电,可以将 ±2.5V的曲线的参考点变一变,即-2.5V看作0V,+2.5V看作 5V,这样就得到了单电源5V供电的曲线。