Part Number: OPA357
峰值保持电路后方接入了OPA357作为跟随器,原理图如下,然而在不接跟随器的情况下他的掉电速度反而比接跟随器的更慢,请教一下原因,有什么推荐的芯片作为跟随器来延长他的保持时间不让他掉电这么快吗?(输入信号为50mv,5Mhz频率的burst脉冲)



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,这两个波形都是OPA357前端输出的波形是吗?在加了OPA357之后输出波形下降?
建议将示波器的水平时间轴/格 调大一些,我想看下一个周期内的波形具体是什么样子的?
您好, .50mv,5Mhz频率的burst脉冲就是前端输出的信号是吗?
也就是这个50mv,5Mhz频率的burst脉冲经过OPA357之后幅值降低对吧?
OPA357的VCC电压是多大?用OPA357做跟随器进行仿真 没有任何问题。
并且从波形来看,不光是幅值降低,看起来有一段时间是发生震荡的,将前端容性负载C19去掉试试呢?
,
不好意思,忘记前端是峰值保持电路了。以下几点可以去验证下:
第一,峰值电容1nF 的C19可能稍微高了,建议改成100pF的再试试。
第二,峰值电容这里接GND也相当于容性负载,建议在前端运放的输出端,二极管和C19之间串联一个22ohm的隔离电阻增加稳定性。
第三,最主要的应该是峰值保持电路的器件MAX43的压摆率不足够高,这里应该使用压摆率尽可能够高的运放,以便在输入超过前一个周期的保持电压时保证第一级跟踪输入。如果手头上有slew rate高的运放,可以替换对比看下。