This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV3601: TLV3601比较器输出方波失真是什么原因

Part Number: TLV3601


比较器的输入是一个脉冲(偏置600mV,幅值300mV,脉宽400ns,上升沿2.5ns),参考电压656mV,然后输入到TLV3601芯片里,输出变成了一个失真的方波

然后又把输入改成一个方波(直流偏置2V,幅值1V,1MHz),然后输入到TLV3601芯片里,输出依然变成了一个失真的方波

现在不知道问题在哪儿,因为仿真是正确的,求大神指点一下,万分感谢!