Part Number: OPA828
看到一些精密仪器的电路运放好像特意设计成非对称电源供电,比如+14v、-17v这种,请问运放非对称电源供电有什么好处吗?信号摆幅不超过正负7v
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
运放的供电电压范围决定了运放信号输入和输出范围。在满足运放规格的前提下,一般是根据输入和输出信号幅值范围和现有的电源电压等级来设计运放的供电电压。如果您需要处理的信号幅值范围相对于0V来说不是对称的,而使用对称电压给运放供电可能满足不了运放的规格,那么就需要使用非对称电源给运放供电,比如运放最大供电电压是32V,而您需要处理的信号幅值范围是-18V ~ +10V,那么您就要使用非对称电源供电,因为使用±18V超出了运放的规格范围,此时您可能需要使用-18V和+10V给运放供电,如果所使用运放不是轨至轨输入的,那可能需要使用-20V和+12V给运放供电才能满足输入信号的范围。
设计时,需要考虑运放输入和输出信号的幅值范围,运放允许的最大供电电压和现有的电源电压等级等,要综合考虑。