Part Number: XTR111
您好,我想请教一下根据公式Iout=10(Vin/Rset) 如何能使0-5V转换成4-20mA,我输入0V怎么才能变成4mA ,不太明白,如下图原理图,是否需要改进让它能从0-5V转换成4-20mA,还是说只能通过DAC电压输出0.8V-4V能确保输出4-20mA 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,按照Iout=10(Vin/Rset)这个公式我们可以看到,0V输入只能输出0mA,是不可能输出4mA的。
并且XTR111内部是没有搭建电路将0V输入可以输出4mA输出的,在datasheet中的Page17也有介绍:
通常的方法是通过外部分压电路将0V输入抬高,使得到达XTR111的电压不等于0,这样才能保证输出能达到4mA。
Figure43举了个例子,0~5V输入抬高到1~5V输入给XTR111作为输入。


我们还是要通过Iout=10(Vin/Rset) 这个计算输出电流,也就是说0V输入是得不到4mA输出的, 0V输入0mA输出。
换句话说,要想得到4mA输出,那么Vin就不能是0V。我们只有通过建立外部电路,使得前端输出的0V通过抬升到一定电压到XTR111的输入端,才能保证得到4mA的输出。
比如Rset=2Kohm,Iout=4mA,那么Vin=0.8V即可,或者其他Rset的值都是可以的,比如1V输入,4mA输出,需要2.5Kohm的Rset电阻。
所以DAC的输出可以不改变,我们可以按照Figure43的电路,在DAC的输出和XTR111的输入端建立分压电路,使得DAC 0V的输出抬升到一定电压给XTR111的输入。

①感谢耐心解释,根据XTR111的开发板分析,就像您解释的DAC输出=0V 时候通过外部电路的分压电阻和XTR111的内部基准电压(5V)使其抬升到1V ,在根据公式Iout=10(Vin/Rset) 得到4mA 这点明白了非常感谢。
②但是根据①的内容我又产生了疑问,如果根据这个开发板的原理图分析,如果DAC输出的VIN=0.5V,这个分压得到的1V和实际DAC输入的0.5V是怎么个关系,还是说根据公式Iout=10(Vin/Rset) Iout=10(0.5/2490)=2mA 吗?如附件所示,我需要在DAC输出0-5V时候使XTR111在4-20mA内成线性关系(在不改变DAC输出的情况下)是否可以实现。
如果DAC输出的VIN=0.5V,这个分压得到的1V和实际DAC输入的0.5V是怎么个关系,还是说根据公式Iout=10(Vin/Rset) Iout=10(0.5/2490)=2mA 吗
根据公式,比如DAC输出0.5V,要得到4mA输出,我们可以去选择Rset的值使其得到4mA的输出。
4mA=10(0.5/Rset),得到Rset=1.25Kohm。
那么这个VIS是如何计算的
Vis指的是IS引脚的电压。指的是外接晶体管的源极。

可以参考Figure17的曲线,可以发现当输出电流越小,接近0V时,Vis的电压就接近Vsp的电压。