This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA301: 电流采样类的放大器的压摆率和通用运放的压摆率测试方法一样吗?因为电流采样放大器一般放大倍数都固定了且比较大如果输入给一个阶跃大信号,那么放大器输出就达到电源轨电压了

Part Number: INA301


电流采样类的放大器的压摆率和通用运放的压摆率测试方法一样吗?因为电流采样放大器一般放大倍数都固定了且比较大,如果输入给一个阶跃大信号,那么放大器输出就达到电源轨电压了,此时压摆率值测的准吗?如果给一个小信号,压摆率似乎达不到规格书的典型值。

  • 您好,

    INA301的压摆率可以与通用运放的压摆率一样测量,具体您是怎样测量的?INA301供电电压是多少?使用的INA301 增益是多少?您可以输入一个正好使其输出不饱和且幅值较大的阶跃信号,比如供电电压5V,增益20倍,对应的输入5/20=250mV,因为输出不能完全达到电源轨,您可以输入240mV的阶跃信号:

    计算SR时,选择10%至90%的幅值变化范围,比如输出幅值由0.5V变化至4.5V需要的时间为Δt,那么SR=(4.5V-0.5V)/Δt

  • 谢谢,之前时我测试方法问题,感谢解答