This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tlc2652

Other Parts Discussed in Thread: TLC2652

   TI的老师,tlc2652应用中说在画电路板时,它的的输入引脚必须做GUARD环保护,请问我围绕输入引脚画一个导线环路,那这个环路应该接通地还是接通别的?

其次我在TI下载的tlc2652PSPICE模型是.101和.102结尾的文件,请问用仿真软件怎么处理才能仿真?

  • Degradation from capacitor leakage becomes more apparent with the increasing temperatures. Low-leakage capacitors and standoffs are recommended for operation at TA = 125°C. In addition, guard bands are recommended around the capacitor connections on both sides of the printed circuit board to alleviate problems caused by surface leakage on circuit boards

    既然是信号隔离和保护用的, 应该接地

  • 你好,关于GUARD环保护设计,请参考下面应用手册 的“4.2.2 Guards and Shields ”部分:

    http://www.ti.com/lit/ug/snou004/snou004.pdf

  • 关于模型问题,试着把尾缀改成.txt的文件,然后在导入试下,参考这个帖子:

    http://www.deyisupport.com/question_answer/analog/amplifiers/f/52/p/73514/178849.aspx#178849