This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA380: 我用OPA380作为光电二极管的I/V转换电路,为什么仿真结果是这样的

Part Number: OPA380


你好,这个OPA380的datasheet,上面说,供电电压是2.7-5.5v,我给OPA380的供电电压是5V,然后按照datasheet进行搭建电路仿真,datasheet里面的RF最大可以为10MΩ,可是我用2MΩ作为RF的时候,输出就已经失真了,这是为什么呢?

我给电流发生器设置的是带有2.4uA偏置的30KHz 振幅为2.4uA的正弦波,如图示,我的TIA电路如图示,仿真波形如图示:

                      

为什么当RF=2MΩ 的时候,输出感觉是一条线,正弦波的输出幅值范围是4.59~ 4.58V,     如果 RF=1MΩ 的时候,     为什么输出曲线的峰谷不是0V,而是1.8V左右? 下图为RF-=1MΩ时候的仿真图,而且为什么输出的波形第一个脉冲的波峰值高于其他的波峰值?