This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这是OPA322用于光电放大的文档:光电二极管放大器电路 (Rev. A) (ti.com.cn)
这是我用TINA搭建的和PDF一样的电路:其中信号源是带有1.2uA直流偏置的1.2uA的20khz的正弦波,如图示。 我经过仿真,发现输出信号的最大幅值到不了4.9V,而且最低点也到不了0.1V,如图所示,这是为什么呢?
您好,我用TINA仿真了下,20Khz的频率时和您的结果类似。
降低频率,幅值变大。下面是5Khz时候的波形,可以看到已经接近4.9V和0.1V了。
当频率降低到100Hz的时候几乎没有差异了。
所以看起来好像该模型的最大增益峰值在10Khz左右。如果将补偿电容改为fA,能解决这问题,我仿真了下结果相符。
补偿电容的范围有计算公式吗?我不知道该怎么选它的值,如果我的信号是30KHz,那我的补偿电容又应该怎么选呢? 还有就是OPA322 和 OPA380 哪一个作为30KHz的光电二极管信号放大电路比较好?
关于补偿电容的计算,可以看下附件这篇关于“跨阻运放指南”这篇应用手册。
还有就是OPA322 和 OPA380 哪一个作为30KHz的光电二极管信号放大电路比较好?
OPA380的带宽更高一些,光电二级管因为是微电流,所以选择做光电二极管放大时主要考虑输入偏置电流的影响,我看了下OPA380的最大Iib为50pA,OPA322在25度时候最大只有10pA,并且OPA322 相对更新一些,可以根据上述应用手册计算下-3dB带宽,如果带宽足够的话,我更推荐OPA 322.