This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV1805-Q1: 供电后不正常工作

Part Number: TLV1805-Q1
Other Parts Discussed in Thread: TLV1805

DATESHEET
如上图按照TLV1805 datasheet设计出来的原理图以及画的PCB,生产出来的实际板子完成贴片后,上电后芯片不能正常工作,电源供进去电源箱没产生电流,使用信号发生器将500KHZ,0.8%占空比,3.3V方波信号供进去没有反应,请问一下是什么问题?
  • 您好,

    反向输入端 3脚,您是打算接直流电压2.5V是吗?接直流电压2.5V需短接C1,因为电容隔直,比较器的3脚相当于浮空。

    您使用的参数与datasheet中的一致,因此两翻转阈值也一致,可以看出一个阈值是1.675V,一个是3.325V,也就是说输入从低电平变化到3.325V时,输出才有低变高电平,但是您的输入最大才3.3V,因此输出是不能切换到高电平的,因此您需要改变设置的迟滞电压,或增加输入电压。

    datasheet 7.4.1.2部分也给出了两翻转阈值的计算公式,如下截图所示:

  • 您好,C1我设置了短接的,给的是2.5V,但是芯片依然不正常工作。我现在的问题是电源供上5V的电压后,电源箱上没有显示电流,意味着芯片没有正常工作,我不太清楚是我的LAYOUT有问题还是设计的电路有问题

  • 如上所述,比较器一直输出低电平,对负载没有驱动电流,其功耗很小,应该是uA级的,电源箱上显示的电流最小是1mA,因此可能是测量不出来。

    所以还是建议您修改这个 3.325V翻转阈值,或者是增加输入电压再测试看输出怎样?

  • 您好,这个芯片的功耗能这么低吗,我不太清楚,我刚刚增加了输入电压,还是没有产生电平翻转,是否是其他原因

  • 您好,还在吗

  • 您可以用示波器同时测量比较器2.5V电压、输入信号波形和输出端的波形吗?我想同时看下两输入信号和输出信号具体是怎样的