Part Number: TLV1805-Q1
Other Parts Discussed in Thread: TLV1805, , TLV1811, TLV1811-Q1, TLV9031-Q1
输入频率大于3Khz的4V电压,0.8%占空比方波信号时,信号消失,在1~3Khz频率下,信号正常输出,但是输入频率大于4Khz后信号直接消失变成低电平。以下图片是在1Khz的频率下TLV1805输出的波形,只要输入波形频率大于3Khz,信号就会消失



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV1805-Q1
Other Parts Discussed in Thread: TLV1805, , TLV1811, TLV1811-Q1, TLV9031-Q1
输入频率大于3Khz的4V电压,0.8%占空比方波信号时,信号消失,在1~3Khz频率下,信号正常输出,但是输入频率大于4Khz后信号直接消失变成低电平。以下图片是在1Khz的频率下TLV1805输出的波形,只要输入波形频率大于3Khz,信号就会消失



您好,
输入频率大于3Khz的4V电压,0.8%占空比方波信号时,信号消失,在1~3Khz频率下,信号正常输出
那说明工作翻转速率大于了 TLV1805-Q1的可以支持的最大翻转速率,您需要可以支持更高速率的比较器,您可以在下面链接选择更高速率的比较器,如下截图所示:
https://www.ti.com.cn/zh-cn/amplifier-circuit/comparators/overview.html

TLV1811-Q1 的工作电压满足您的要求,TLV1811-Q1 是push-pull输出,其输出上升时间典型值是15ns(CL=50pF),工作翻转速率典型值 500K(VID = 100 mV, CL = 50 pF)。典型值是满足您的要求,但具体还要看您的应用,因为参数刚刚满足您的要求,没有余量,所以还要考虑过驱动电压VID和电容性负载这两个主要参数。CL与您的PCB设计有关。并且,TLV1811-Q1的传输延迟典型值是420ns比 TLV1805-Q1的还大:

您可以看下 TLV9031-Q1,下面是它们的参数对比