主要用于APD激光测距的接收模块,包括一级的TIA电路和二级放大电路
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
输入信号频率范围是多少?输入电流幅值范围是多少?C5 2.6pF是APD的结电容是吗?
不建议在运放反向输入端接电容 C8,这会引起运放电路稳定性问题。稳定性问题您可以使用TINA进行仿真。
下面是关于光电二极管放大电路的参考设计,您可以参考下:
1、1 MHz, Single-Supply, Photodiode Amplifier Reference Design
请问您,稳定性问题应该看什么参数
具体您可以看我上面给您的链接文档,即:1 MHz, Single-Supply, Photodiode Amplifier Reference Design

关于输入和输出范围,看到您将TIA的同向输入端设置在了3.8V。您的输入电流范围是0-15uA,增益是16K(8K+8K), 那么输出摆动幅值是0-15uA*16k=0~0.24V
输出基准电压3.8V,那么输出幅值范围是3.8V ~4.04V。这已超出了运放在25℃时的最小输出摆幅3.95V,因此不建议您将TIA的同向输入端设置在了3.8V,建议您调小一些。
另外,您的输入信号频率为3K,CF选择160fF//160fF=0.08pF,电阻为16K,电路带宽为124Mhz,比需要的3KHZ大太多,电路带宽设置的太大了,容易耦合进高频干扰。