您好,我现在需要设计一款输入电流为0-1000uA的APD前放电路
当输入电流超过OPA855的3VPP的幅摆的时候,会出现如下图所示的震荡,请问该如何解决
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
当输入电流超过OPA855的3VPP的幅摆的时候
如下截图所示,OPA855在单电源5V供电时,其输出电压摆幅典型范围是1.1V~4V,摆幅峰峰值不到3V,因此上述振荡可能是输出范围超出OPA855规格造成的,您尝试减小电路增益,将输出限制在1.1V~4V以内,比如1.5V ~3.5V之间,看振荡现象是否消失?
您好,饱和输出的时候不确定会输出什么,有的运放输出会削顶,有的运放会发生输出极性翻转。不建议您将运放设置工作在这种非线性状态下。
另外,新的问题建议您发新帖。