Other Parts Discussed in Thread: OPA3S2859
您好,我基于贵司的OPA3S2859芯片进行了跨阻放大器测试,外围电路搭建都合理,电路重点参数如下:
1.供电电压4V(是为了配合FPGA的3.3V控制而设置),符合电压范围;
2.INA+和INB+输入共模电压设置为670mV;
3.INA-和INB-悬空;
4.LTCH_A和LTCH_B悬空;
5.增益电阻分别为:1K(反馈电容1.5PF),10K(0.7pf),100K(无);
问题:输出波形形态正常,但是其反应很不敏感,基本上需要光与光电二极管对射或者用强反射面反射才会有信号输出,否者基本上是不会有信号输出的,我怀疑是不是增益没有起来导致信号不敏感(有个重点是信号底噪很小36mV,太过于小显得不正常,也指向了没有正常放大),或者说芯片其它的一些原因导致。