Part Number: OPA2863
如下电路,输入引脚3的电压为1.496V,测试输出引脚2的电压只有1.482V,理论上输出2引脚应该和输入3引脚的值相同吧或接近,之前用其它运放输入和输出差不超过0.002V,采用OPA2863为什么差0.014V这么多?受哪个指标影响?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想有可能是这个原因造成的,但是我不确定,需要了解U2'和1/2VREF信号的连接或它们是怎样产生的;
U2‘是变压器输出信号是吗?没有连接到其他电路?
1/2VREF是基准电压芯片产生的基准电压?
我在网上找了个相关话题描述,您看下:
https://zhuanlan.zhihu.com/p/627236042