Other Parts Discussed in Thread: TINA-TI, LM2903
Hi TI team,
下图电压的方波,如何用TLC2272或者其它方式转换为UL=0,UH=3.3V,让MCU能够正确的识别,,周期,频率,相位保持不变,谢谢


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,输入信号范围8V ~11.8V, 输出为9.2V~13.2V。
那么可以计算Gain=(13.2-9.2)/(11.8-8)=1.053V
然后您可以根据这篇文档的电路,参考里面的公式去计算对应的四个阻值,可以假设R1=R4=1Okhm,Gain=1.053. Vref为1/2VCC, 假设16V单电源供电,Vref=8V。
然后直接使用里面的公式去计算R2和R3即可。
我计算下来R2=2110ohm,R3=400ohm。但是输出电压到11.47V之后饱和了。我再计算下,应该是哪里出错了,您这边也可以计算下:

您好,我才看到您要输出0~3.3V是吗?
我可能理解成8V ~11.8V, 输出为9.2V~13.2V的要求了。
您好,抱歉回复晚了,上周后面几天请假了。
我用LM2903比较器仿真了下,是可以实现的。仿真结果如下: