OPA334放大器经常出现焊接完毕,电路板第一次上电测试就出现OPA334故障,查电路设计,单电源5V,最大共模电压小于2.1V,采用白光焊台手工焊接,静电保护措施均设置,焊接温度350度。请专家分析原因
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Wei
根据你描述的现象,请帮忙确认:
1)检查应用电路是否有问题,请提供电路图;
2)排查OPA334故障现象,如是否烧掉(管脚处有起泡?)、管脚的IV特性是否正常?若是这个原因,则排查你上电过程是否有EOS。
regards,
Steven
对于焊接,建议将烙铁温度降到300℃以下,在datasheet中ABSOLUTE MAXIMUM RATINGS部分显示,Lead Temperature (soldering, 10s) 为+300°C,其次, datasheet中,PACKAGING INFORMATION部分,MSL Peak Temp中的peak solder temperature显示是260℃,故建议降低焊接温度。
具体的焊接要求可以参看下面链接的文件:
如果能排除焊接问题的话,建议提供OPA334的电路及相关数据以供分析。