大家好,问下:
在使用TI的LMV358进行电压跟随设计的时候,当输入3.3V时(供电电压=3.3V),输出仅有2.7V左右,并不能实现轨到轨输出啊?是我理解问题还是芯片本身问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输入3.2V 输出也能3.2V (供电3.3V ) 做电压跟随用的 ,只能用rrio吗? 是轨到轨输入输出/
RRIO指的是输入输出都能轨到轨,也就是说输入输出都能到达电源轨,如果供电3.3V,输入输出都3.2V的话,普通的运放输入输出范围可能没这么大,最好使用RRIO肯定能实现。
OPA378可以,2.2~5.5V供电范围,RRIO,并且单位增益稳定。
说是轨到轨,也不是完全能到电源轨,根据负载的不同而不同,像我说的OPA378,10Kohm的负载,输出最大幅值和电源轨相差在6mV左右,比如5V供电,最大输出为4.994V,比较了下LMV612,在相同负载下,LMV612输出的要偏离电源轨稍微大一些,datasheet中没有给出3.3V的情况,5V的时候600ohm负载最大输出4.89V。 3.3V的情况需要做下试验验证。