This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4521输入端电压不正确问题请教

Other Parts Discussed in Thread: THS4521, ADS1274, OPA2734

用THS4521+ADS1274测量模拟信号,根据《使用负输入电压的单电源全差动放大器驱动 ADC》,想用这个电路测量正负的信号,不知是否可行。

现在测试发现,对THS4521输入端,直接接个电阻到地,其输出端还是有1.6V的差分电压,电路图如下。

图中20K电阻,实际焊接的是1K,芯片为THS4521,signal_C,是信号输入端,现在用一个3K电阻,连接到电源地,THS4521输出端,连接到了AD的输入端,测试发现,R156左侧电压为1.6V,想请教下原因,谢谢。

  • 你好,这是因为你的运放差分运放,要求正负端电阻的比例相同,即R157/R156=R159/R158

    你用3k电阻接地,相当于R156从1k变成了4k,所以会使得输出不为0

    可以参照附件中TINA仿真模型

    FDA.TSC
  • 请问你为何要使用3K的电阻接到低呢?信号源内阻?

  • 感谢回复。

    我前端本来接的是运放的电压跟随,输出到THS4521,传感器是无源的,发现接上传感器,输出一直有电压,把传感器去掉,在电压跟随器输入端,直接用电阻接到地,输出还是有电压。

    之后把运放OPA2734拆掉后,就把信号输入端直接接到THS4521上了(3k电阻接到地),

    想请问,我这种信号接电压跟随器,再接THS4521的用法是否有问题,如果有问题,是否可以把传感器直接接到THS4521上,

    能力有限,还请不吝赐教,非常感谢!