Part Number: LM324
Other Parts Discussed in Thread: NE555, LM339
输入端为三相交流半波正路后的波形,经电阻R13(348K)和电位器R10(10K),二极管V25,电阻R11(10K)连接至N相。第2张图片中黄色为运放LM324同相端电压的波形,上电后3分钟左右存在偶发的电压抬升的现象(半波整流的电压并未改变,二极管V25的电压也未改变),请问与运放LM324有关吗?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好。N3是图中的LM324,供电电压是15V,由LM7815提供,没有负电源,LM324的4脚接15V,11脚接GND。LM324在此处当比较器使用。同相端突变的时候,反相端电压很稳(V7提供6.2V的基准)。同相端突变时候产品没有接负载,附近也没有其他干扰源,在室温条件下,检测过交流电源的品质很好,没有出现单相突变的情况。同向端的布线长度51mm,反相端的布线长度40mm。这是个老产品,整个产品主要由三极管,二极管,电阻,稳压管,NE555,比较器LM339,运放LM324,电容,继电器,LM7815组成。继电器平时是不通电的。NE555用于频压转换电路。
产品工作8年后可能故障,
产品工作8年前不会出现此故障是吗?如果是这样的话,感觉是芯片损坏造成的。
R10和运放的同相端是等电位点,它俩是同一个电压。
我的意思是R10电位器两端的电压是否有改变?
现在可能有问题的是电位器R10和运放LM324,确定不了是哪个。
如果R10电位器两端的电压没有改变,那应该可以排除R10的原因了
故障后波形有没有再抬升或者恢复,
如果这个抬升现象是固定时间发生的,后续可以恢复不再发生,那么很可能是干扰问题。但是您描述说“产品工作8年后可能故障”,这不像是干扰造成的。
如果其他器件两端电压都没有改变,那么很可能是运放损坏的问题了。