Part Number: LOG114
在使用EVM板时,空载状态下Vout有370mv的输出,按照EVM板文件插入光电二极管时电路输出还是370mv(此时室内有灯光,二极管有电流产生),随着光强增加一段强度内输出无反应,光强加到一定程度时输出从370mv跳变到1.4v,之后输出正常随光强增加而增加。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LOG114
在使用EVM板时,空载状态下Vout有370mv的输出,按照EVM板文件插入光电二极管时电路输出还是370mv(此时室内有灯光,二极管有电流产生),随着光强增加一段强度内输出无反应,光强加到一定程度时输出从370mv跳变到1.4v,之后输出正常随光强增加而增加。
在使用EVM板时,空载状态下Vout有370mv的输出
您这里“空载状态”是什么意思?是指悬空EVM板的I1输入端吗?如果是这样的话,不建议做这样的测量,因为悬空模拟输入端会耦合周围的电磁干扰造成不确定性输出,还有可能输入范围超出规格范围损坏芯片。
按照EVM板文件插入光电二极管时电路输出还是370mv(此时室内有灯光,二极管有电流产生)
您是焊接好光电二极管,然后EVM板上电后VOUT默认输出是370mV吗?此时测量VLOGOUT输出是多少?VLOGOUT 应该约等于下面计算公式:

因为I2= 500 nA,如果您输入500nA到10uA之间电流,VLOGOUT 电压在 2V~1.512V
另外,2V偏置电压输出正常吗?
建议您先使用电阻代替光电二极管产生输入电流,因为 LOG114EVM User Guide 中的第5部分 Verifying Results 有相应测试结果,您可以进行对比。