对于VCA810,它的Vc,控制电压是-2V到0V,那么数据手册上那个自动增益控制(AGC)电路中,的V-的取值应该为多少呢?若V-=-5V,那么,是否可以通过改变分压电阻,使得Vc的最大负电压不能超过-2V。另外,OPA820的输出摆幅为正负3.5V,那么是否是在AGC完成时,Vc处电压都不会超过其(-2~0)的范围,因为电容的存在。
另外,VCA810的输入输出最大不能超过2V是吧!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.