This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA564: 上电发热严重

Part Number: OPA564

您好,Ti专家

   我们使用OPA564产生-0.5V到-3V的输出,输入采用的是DAC控制。我们发现上电后OPA564就开始发热,开始怀疑是上电DAC就输出了导致功放输出而发热,

但是我们去掉R198后,功放还是同样的发热,请问这种状况正常嘛?OPA564这部分的原理有上面问题嘛?

  • 您好,

    发热时输出是不是振荡了?如果是的话,很可能是电路不稳定造成输出振荡引起的发热。不建议在运放输出端接C187和C186电容,因为运放驱动容性负载的能力是有限的,PCB 走线也会产生一定的寄生电容,负载电容太大的话就会引起运放输出振荡,您去掉C187和C186电容看是否可以解决上述发热问题?

  • Hi Amy Luo

         我试过去掉电容,效果不大。请问输出振荡怎么判断?

  • 用示波器测量输出波形对输出波形判断

    测试时运放输出端接的是什么负载?

    另外,去掉R198后,运放的同向输入端就悬空了,模拟输入端悬空的话会耦合周围的电磁干扰,因此测试时请将运放同向输入端有确定的电平电压。

    C176电容值太大了,一般是pF级的,您去掉C176电容或换pF级电容后测试结果怎样?

  • 您好,Amy Luo

       目前是不接任何负载,给±5V电给功放,它就开始缓慢发热。也没发现任何短路的地方。就是上面贴的原理图那样。我们的负载在另外一块板子,那块板子都没连接上。

  • 运放同向输入端是否有确定的电平电压?

    您去掉C176电容或换pF级电容后测试结果怎样?

    您测试了几块电路板是这种现象?是否可以多测试几块板子以排除焊接问题?