小白求助,OPA564最大电流可达1.5A,Rset我设置的7.5K,为什么输出电流只有微安级啊?附Tina仿真电路,输入信号为正弦波,频率387Khz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,麻烦 把您的TINA reference model附上,我这边仿真下看看。
输出电压不对,所以输出电流也不对,+-2V的输入信号,输出怎么只有1.42mV。
您可以直接参考主页上提供的参考电路:
输出电压均方值1.42V,负载电阻10K,那么电流均方值1.42/10K=0.142mA=142uA 没问题。
您根据Rset设置输出电流限值,那么也能计算出相应的负载电阻来。
或者您根据负载电阻,想得到一定输出电流,去决定Rset的值。