Part Number: INA180-Q1
Other Parts Discussed in Thread: INA180

手册里只说了Vout大于0.5V的增益误差,0mV<Vout<0.5V时,是什么情况?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,参考Table9-2对几种不同器件的gain error factor,根据外部串联电阻Rf先计算出gain error factor,然后再根据公式5得到gain error。

按照公式计算,增益误差和Vsen的大小无关,为啥手册里指写了0.5V<Vout<(Vs-0.5)V的增益误差。
当0V<Vsen<(0.5/G)V时,其增益误差范围是多少?Vsen和Vout的线性度能否保证?
为啥手册里指写了0.5V<Vout<(Vs-0.5)V的增益误差。
您好,这个给我的第一感觉是因为输出电压距离供电电源轨的压差。
也就是说,Vout的电压范围在GND+0.5V<Vout<Vs-0.5.
因为即使是轨至轨的运放,距离运放电源轨还是有些压差的,我看了下INA180,距离正压轨30mV,也就是输出能最大达到Vs-0.03V.
最低5mV,也就是输出最低电压GND+0.005V,即输出最低电压达不到0V,为0.005V。所以0.5V<Vout<(Vs-0.5)V这个条件还不是输出电压范围的。
所以也就是说想知道在0.005V到0.5V这个范围内的增益误差,是不是
已确认,就像我上面描述的,虽然输出电压范围GND+0.005V<Vout<Vs-0.03V
但是对于INA180来说,最佳的输出电压范围也是0.5V ~Vs-0.5V,能保证它的线性工作范围。 在这个条件下也是Gain error 最小的。
我看了下其他仪表运放,关于gain error的参数,基本上测试条件都是Vout的输出电压范围。