Part Number: AMC1301
我想请教一下关于AMC1301输入端口的问题,通过查看数据手册,输入端口电压范围是±250mv,我所做的设计需要进行母线电压采样,我给的电压是60V,经过分压后得到的电压是250mv,但是与AMC1301VINP连接后,电压就不是250mv了,这是什么原因,谢谢。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
这是由于AMC1301器件的差分输入阻抗为 22kΩ,导致了上面显示的误差:

建议按照下面应用手册中步骤设计电路分压参数,并在放大器反相端子引入串联的 R3' 可以减少偏移误差和增益误差。
| 具有 ±250mV 输入和差分输出的隔离式电压测量电路 (Rev. A) |