Part Number: LOG114EVM
Other Parts Discussed in Thread: LOG114
在图中红圈位置接进不同阻值电阻,实测输出值比仿真值高。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,看了下这个阻值列表,不知您的电流是多大的,换句话说输入电压是否接近Log114的输入失调电压,因为离 LOG114的输入失调电压越近,输入失调电压就越会降低电流生成精度,那么输出偏离线性输出的误差也就越大。总之我们要使用的阻值,尽量使得U=Iin*R 远高于输入失调电压,避免因失调电压带来的误差。
这是在零偏压下使用的,这个EVM板的输入电流可以在10nA-10mA之间,我接入二极管发现输出与理论有差距,我就只接入电阻来看这个差值。芯片里A1的失调很大,A1的正负输入端跨接在3Ω和接入的电阻上,感觉是这个失调的影响很大,但不确定是不是。
是的,A1的输入失调电压很大, 所以根据EVM板的输入电流可以在10nA-10mA之间的话,Rtest=1K的话,1uA的电流电压就为1mV。 那么1Kohm阻值的条件下,小于1uA的电流产生的压降就小于1mV低于失调电压,更别说您选的其他几十几百ohm的阻值了。
我有两个二极管,一个内阻1MΩ,一个内阻200Ω的,大内阻的一直能正常工作,小内阻在大电流可以正常工作,小电流就不行了,受A1影响太大,这种问题有什么办法解决吗,还是说只要用了LOG114,这个问题就没法克服。
我有两个二极管,一个内阻1MΩ,一个内阻200Ω的,大内阻的一直能正常工作,小内阻在大电流可以正常工作,小电流就不行了,
您的这个验证更进一步说明了失调电压的影响降低了精度。
那使用log114这款可能就是有这个局限性,因为我们要避开失调电压的影响。

评估板手册中写到单电源供电需要2 V的电平移位以保持LOG114内部的节点适当偏置,log114芯片的手册中给出的单电源供电的应用中用的是内部的2.5v,这里用哪个比较合适?
您好,您是指的R7这里,这里的R7和R8作为分压电路将Vlogout通过这个分压之后输出的信号给A4的同相端 ,A4的反向端输入高电流线性校正信号,结合输入信号和线性校正信号由放大器 A4及电阻 R5和 R6完成,得到Vout的输出。

关于这部分的电路,可以参考数据手册Figure3, 内部运放A4的输出架构。

上面提到的另一个问题呢,评估板手册中写到单电源供电需要2 V的电平移位以保持LOG114内部的节点适当偏置,log114芯片的手册中给出的单电源供电应用电路中,运放用的是内部的2.5v电平
是的,都是可以的。手册上直接使用的Vref=2.5V作为偏置电压使得输入电压被抬高到Log114的电压范围内。
EVM使用的2V,都是可以的,只要保证单电源条件下,输入内部运放的输入电压在范围内(>=1V)即可.