This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
当电源Pin的VCC为2.5V时,两个输入PIn电压按照要求应在0.5V(2.5V-2.0V)范围内才对。实际线路设计如下。
正常上电工作后,第2Pin,第3Pin 之间的电压差很小 只有80mv(0.32V-0.24V);
请问:一般来说这两Pin的电压差多少合适 以及 这么小的电压差会不会存在什么异常(比如ESD测试时导致其输出截然相反);
您好,
因为 LM393B是比较器,两输入端电压在规格范围内就行,它们的电压差是多少取决于输入信号和阈值设置。不会存在什么异常。