This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ALM2402-Q1: 实现稳定电压参考电路

Part Number: ALM2402-Q1


您好,

需要用ALM2402-Q1实现以下功能:
ALM2402输出端串接一电阻至可变电压源,要求ALM2402输出端稳定在0.2V直流电压(精度 10%左右),SINK电流最大300mA电流。

想问以下设计能否满足上述要求:
1. ALM2402供电3.3V

2. ALM2402任意一通道接成单通道增益为 0dB的正向输入放大器,输入端接0.2V输入。

上述电路是否可行?