Part Number: INA826
使用了两个INA826AID做多级放大,第一级输入为一个差分信号,放大倍数20倍。第二级将第一级的输出信号与地作为差分,放大50倍。第一级放大后的输出电压与差分信号的差值呈20倍关系,第二级的输出信号在差分电压较大如44mV时,输出电压为1.6V左右,不是设计的50倍放大。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA826
使用了两个INA826AID做多级放大,第一级输入为一个差分信号,放大倍数20倍。第二级将第一级的输出信号与地作为差分,放大50倍。第一级放大后的输出电压与差分信号的差值呈20倍关系,第二级的输出信号在差分电压较大如44mV时,输出电压为1.6V左右,不是设计的50倍放大。

您好,
第二级由于输入共模电压限制,输出达不到正常的44mV*50=2.2V,如下截图所示,

上图是使用工具 Analog Engineers Calculator直接输入相关参数(器件型号、供电范围、增益范围、Vref电压、共模电压)给出的输出范围,为验证输入范围的正确性,您可以在下面链接下载这个工具:
https://www.ti.com/tool/ANALOG-ENGINEER-CALC?keyMatch=ANALOG%20ENGINEERS%20CALCULATOR
为更清楚的使用这个工具,您可以点击截图中的Help 按钮查看说明。