This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV271: 关于3.3V供电做3V电压跟随器的问题

Part Number: TLV271


请问TLV271在3.3V供电的情况,可以做电压跟随器跟随3V信号吗?

这是官方的仿真文件,第一个电路是官方仿真电路,第二个和第三个是我做的电压跟随器,输入信号为3V,希望放大器输出为3V。

第二个电路,TLV271的供电电源为5V,从仿真结果看是没问题;

第三个电路,TLV271的供电电源为3.3V,同样输入3VDC的情况下,其输出结果仅为2.8V左右。

有没有朋友在3.3V供电的情况下做过实际的电路呢,或有这样的问题吗?