Part Number: INA199
HI TI
使用INA199用于监测负载设备电流,电路如下,VBAT是电池电压,ADC_POWER_ECS1是直接连接到设备的,在没接入负载情况下,系统能检测到大概200mA的底噪电流,请问如何改善这个问题?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA199
HI TI
使用INA199用于监测负载设备电流,电路如下,VBAT是电池电压,ADC_POWER_ECS1是直接连接到设备的,在没接入负载情况下,系统能检测到大概200mA的底噪电流,请问如何改善这个问题?

您好,
在没接入负载情况下,
是指差分输入为0,共模输入为VBAT吗?如果是这样的话,因为VREF接地,理想输出应该是0V,但是INA199输出达不到0V,即它有最大输出电压摆幅限制,如下截图所示,输出到不了GND,有一个最小输出如下截图条件下典型值为5mV,这样计算输入电流就不会是0A。

输出电压摆幅还受输出电流的影响,具体见Figure 6-6 特性曲线 Output Voltage Swing vs Output Current 。
您可以通过将VREF接一个电压,使得输出以VREF电压为基准摆动以将输出限制在INA199输出范围内。