如下设计,如果VSP是24V供电,想知道能接多大的负载,如果0~2mA它能带动10kΩ的负载吗,从Vsp到下面会有多大的压降
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,参考数据手册针对IS 和VG引脚的电压介绍,Vis不会高于Vsp - 6.5V。 VG不会高于Vsp -18V。
所以如果我Vsp 给24V的话,2ma的恒流大小是不能接10kΩ的负载的,因为此时Vis低于17.5V,Vg低于6V,负载两端的电压也是低于6V,是这个意思吗
是的,不能接10Kohym负载,2mA,10Kohm负载,负载两端电压为20V。 即Vg=20V这是不允许的,Vg最高电压为6V。
最大可接负载为3Kohm。