This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA858: 作为平衡PIN管的TIA放大器,输出存在50MHz-60MHz噪声,求各位大侠支招,万分感谢。

Part Number: OPA858

TIA电路如下,P17和P18是两个PIN管,现在的问题是:没有光输入的情况下TIA输出包含50MHz-60MHz的噪声带,如下第二张图;当用手接近R101左侧时(即两个PIN管的公共点),噪声带里立刻出现一个尖峰,大约53MHz,如下面第三张图。更神奇的是:板子上有个网口,用手握住网口附近的网线,噪声也会立刻从第二张图的样子变成第三张图;用手接触网口连接器的外壳(接系统电源地),产生同样效果;

            

这个53MHz的尖峰频率非常固定,我尝试改变反馈支路的阻容,改变R101和R190,改变R196和C298,改变R98和R194,它的频率都不变。因此我认为这不是寄生参数或运放内部参数引起的振荡,应该是TIA耦合了别处的干扰。但是奇怪的是,当我吧R101左边和PIN管断开,保持悬空,反倒没有这53MHz的干扰了。

请教高手指点,不胜感激!