我想请问下LMH6321这款芯片怎样调节输出电流呢,根据芯片手册说改变CL管脚上的电压值就可以从30mA到300mA改变电流,但是用Multisim仿真的时候发现电流并不会变化,只会随着负载的变化而变化,而且输出电压也存在微弱的失真,我的输入电压时5V,10MHz的正弦电压,TI的技术人员能给我点意见吗?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想请问下LMH6321这款芯片怎样调节输出电流呢,根据芯片手册说改变CL管脚上的电压值就可以从30mA到300mA改变电流,但是用Multisim仿真的时候发现电流并不会变化,只会随着负载的变化而变化,而且输出电压也存在微弱的失真,我的输入电压时5V,10MHz的正弦电压,TI的技术人员能给我点意见吗?谢谢
你好,很感谢你的回答,但是我还是没有理解它是怎么放大电流的,当然,根据仿真结果输出电流确实是放大了的,输出电流达峰峰值达到178mA,但我发现CL管脚电压在0.25~7.5V之间变化时这个电流都不会发生变化,根据芯片手册,CL管脚电压在0.25V时,最大输出电路应该只有10mA才对 ,不知道是不是因为仿真无法对这款芯片进行仿真的原因?
1.但是用Multisim仿真的时候发现电流并不会变化,只会随着负载的变化而变化, 这是典型的电压跟随器的特性,限流有些时候在模型中没有包括。
2.输入请并联50欧姆电阻,输出请串联50欧姆电阻,以减小放射失真。
3. 在PCB上测试,限流值是可调的,限流后可能会出现削波失真,请问你是想用限流调节来实现一个什么样的功能?
谢谢
你好,很感谢你的回答,我想请问下你们的评估板可以满足对10MHz,5V的正弦信号的功率放大吗?