Part Number: OPA657
Other Parts Discussed in Thread: OPA847


如图所示,图一图二都家里2.5V偏移。但是图一的交流输出VM1只有20mV VPP,但是图二加上后级放大后,VM1交流电压有1V VPP,请问这是为什么。电流源参数两幅图一致如图一所示。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
但是图一的交流输出VM1只有20mV VPP
图一是正常的,我看电流源是+-1uA的正弦波,反馈阻值10K,那么1uA*10K=10mV。如果没有偏置的话即为+-10mV的输出,现在加了2.5V的偏置,所以输出是以2.5V为参考,20mV峰峰值的输出。
但是实际上,OPA 657的供电电压范围为8~12V,双电源供电为+-4V ~+-6V .所以仿真电路中使用单电源5V供电实际是不在供电电压范围内的。

你好,电路中的LPM7721最大输出为6V。不过之前有个后级采用OPA847的班子,OPA847手册上写的是供电+-5V,那么如果将它作为单电源运放的话,VS=0V, 那么VCC是不是最大就可以接10V了
不过之前有个后级采用OPA847的班子,OPA847手册上写的是供电+-5V,那么如果将它作为单电源运放的话,VS=0V, 那么VCC是不是最大就可以接10V了
OPA847 是的,可以单电源10V供电。OPA847的最大供电电压为+-6V,即单电源供电的话,12V供电。