从INA232的datasheet中看到其input bias current = 10nA(Max), 感觉可以用来测量uA的电流。测量最大30uA的电流,INA232精度能否达到? 输入端是否需要加额外的滤波器?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
从INA232的datasheet中看到其input bias current = 10nA(Max), 感觉可以用来测量uA的电流。测量最大30uA的电流,INA232精度能否达到? 输入端是否需要加额外的滤波器?
您好,
总的误差精度不仅与输入偏置电流有关,还与输入失调、输入共模电压CMRR、供电电压纹波PSRR、增益误差、采样电阻误差等有关:

因此,这与您使用的输入共模电压、供电电压纹波、采样电阻精度、采样电阻值等都有关。
INA232 如下截图所示,输入失调误差最大达50uV,如果您选择较大的采样电阻值,这样shunt电压就占输入电压的主要部分,可以降低误差百分比。但太大的采样电阻会增加功耗,这是一个折中考虑的问题。

输入端是否需要加额外的滤波器?
根据您的测量系统或者说测量信号是否存在噪声或干扰来决定是否加滤波器。具体见datasheet 8.1.4章节 Filtering and Input Considerations描述。