This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3091: THS3091输出问题

Part Number: THS3091



第一个问题:请问这个串联50欧姆是有什么作用吗?它的分压使我的放大倍数衰减一半。
第二个问题:在仿真时,我输出端接入50欧姆的负载,输出的正弦波峰峰值可以到达20V,但是实际电路使用时,输出峰峰值到8V左右就开始失真,如果把负载去掉就可以像仿真一样完美,请问是跟芯片输出端电流有关吗?我想让输出端接入50欧姆负载的同时输出峰峰值能达到20V以上,该怎么做?是要进行二级并联芯片吗?

  • 第一个问题:请问这个串联50欧姆是有什么作用吗?它的分压使我的放大倍数衰减一半。

    是的,加了这个串联50ohm电阻之后,放大倍数减半,这是一种double terminated的应用,像有些放大器的增益是固定的,那么可以通过这种方式使得增益减半,达到应用目的。THS3091的Figure 9-1 为了通过这两个电路来说明load sharing负载共享的应用。可以详细看下3091数据手册9.2.2 Detailed Design Procedure部分的介绍。

    在仿真时,我输出端接入50欧姆的负载,输出的正弦波峰峰值可以到达20V,但是实际电路使用时,输出峰峰值到8V左右就开始失真,如果把负载去掉就可以像仿真一样完美,请问是跟芯片输出端电流有关吗?

    是的,THS3091是一颗高电流输出运放, 可以达到+-310mA,输出电流太大将输出电压拉低。

    我想让输出端接入50欧姆负载的同时输出峰峰值能达到20V以上,该怎么做?是要进行二级并联芯片吗?

    您需要使用这种高电流输出的器件吗?THS3091的输出电流很高,并且带宽相对其他功率放大器也大一些,所以您具体是什么应用

  • 我想使用THS3091这个芯片作为宽带直流放大器的功率放大部分,使负载50欧姆电阻的最大正弦波峰峰值在10M频率下输出能够达到22V

  • 具体电路图上图所示,放大倍数为5倍

  • 是的,THS3091是一颗高电流输出运放, 可以达到+-310mA,输出电流太大将输出电压拉低

    我可以在反馈之前加入电阻作为放大器内部负载来减少输出电流,增大输出电压吗?就像这样

    它的仿真输出和之前是一样的,但我不知道实际电路能否正常工作以到达我的目的

  • 您好, 稍后给您回复。

  • 使负载50欧姆电阻的最大正弦波峰峰值在10M频率下输出能够达到22V

    您好,抱歉回复晚了,参考Figure7-20的曲线,负载为50ohm时,可以看到输出是可以达到+-12V多一点,因此峰峰值为22V是没问题的。

    所以我看了您上面提到实际电路中,输出8V就开始失真了,大于8V饱和了是吗?

    因为参考上面的曲线,THS3091是可以满足要求的。