This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF37D73: 经常烧毁

Part Number: TRF37D73


您好!

我们的电路如下图所示:

但是我们发现放大器TRF37D73经常烧毁,请问这个电路有没有问题?

我们的电源电压是3.3V,经过输出电感L3之后,在输出管脚7上面测得的电压大约为3.2V。查数据手册,TRF37D73的最大电源电压是3.6V:

因此直流电压是在正常范围之内的。但是放大器工作时,RF输出功率可能达到10dbm(也在放大器允许范围之内),此时RF信号的峰峰值为2V,叠加在直流电压3.2V上,最大电压可能达到3.2+2/2=4.2V,超过放大器最大容许电压3.6V。这是否是放大器烧毁的原因?

谢谢!

吴端